freemaster

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

freemaster

1,586件の閲覧回数
danvandre
Contributor I

how does your freemaster gui (or pgm) calculate a frequency from rpm entered in the gu ?

2 返答(返信)

1,491件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Dan.

Generally following equation is applies:

freemaster2.png

You must know scale of frequency. Scale * Q.15.

freemaster.png

For example scale = 1000 Hz, if Q1.15 = 0.4, then frequency is 1000*0.4 = 400 Hz

I hope this helps.
Best Regards,

Iva

1,491件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dan,

It would be helpful if you could provide us more information, which MCU are you using? Are you running a demo project?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信