frdmk66f_lwip_httpsrv_mbedTLS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frdmk66f_lwip_httpsrv_mbedTLS

1,211 Views
a8Chcx
Contributor V

Hi,

I am trying to use "frdmk66f_lwip_httpsrv_mbedTLS" to build my http server.

I disabled "MbedTLS" and "WebSocket", then it works as regular http server. It works fine with sample web pages.

Then, I start using my web pages and works as normal most of time.

1) But, it stop working if load a little bit big files(>2K). It shows "ERR_CONNECTED_TIMED_OUT" on browser. Can anyone tell me how to increase the timeout in project?

2) If I access the server from different machine to connect more session, it stops working? Can anybody tell where the possible problem is and how to fix it?

Thanks,

Christie

 

0 Kudos
Reply
1 Reply

1,189 Views
a8Chcx
Contributor V

Hi,

I did more testing on this sample and found:

1) At the first time loading, it is very slow, only for 2K, it takes more 5s.

2) If I clear history, it loads much fast, less than 1s. I can't understand why?

3) If I press F5, I can see _end_of_heap increased and page refreshing is very slow...

I do not have this issue when I am using bare-metal http server  sample by using RAW API.

Can anybody help me to debug this issue? I really need this to be fixed?

Thanks,

Christie

0 Kudos
Reply