frdm k64 can bus query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frdm k64 can bus query

4,356 Views
kaushikvarma
Contributor I

Hi ,

      I have 2 frdm k64 development boards and I am trying to use CAN bus for making communication happen between the boards. For this I tried flexcan_loopback example in MCUXpressoIDE_10.2.1_795. In the readme part it I saw that PTB16 and PTB17 are to be connected. I couldnt find the pins PTB16 and PTB17 in the board. Can I know from where the output of those pins## taken. Thank You. 

0 Kudos
Reply
6 Replies

4,108 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

If you want to use CAN bus for making communication happen between the FRDM-K64F boards, CAN Transceiver is needed.

There is flexcan interrupt_transfer example in SDK_2.5.0 of twrk64f120m.
You can see this example need Two TWR-SER boards in readme file.(The CAN Transceiver is on TWR-SER board)

SDK_2.5.0 twrk64f120m flexcan interrupt_transfer.png

TJA1050T TWR-SER.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,108 Views
vimalprasath
Contributor II

is there any way i can connect one of the boards to PC via CAN-USB Convertor?

do we have any CANBUS based serial terminal so that transmit data and check data received from one Board?

Thanks,

Vimal

0 Kudos
Reply

4,108 Views
mjbcswitzerland
Specialist V

Hi

See https://www.youtube.com/watch?v=Ha8cv_XEvco
for Komodo CAN-USB

Regards

Mark

0 Kudos
Reply

4,108 Views
vimalprasath
Contributor II

Thanks Mark Butcher,

This will really help me a lot.

but i feel like Komodo CAN-BUS is too costly.is there any similar product in low cost??

0 Kudos
Reply

4,108 Views
mjbcswitzerland
Specialist V

Hi

There are many such analysers available if you do a search, although you will need to check out what features you need and what they offer. See for example:

https://www.8devices.com/products/usb2can

Regards

Mark

0 Kudos
Reply

4,108 Views
mjbcswitzerland
Specialist V

Hi

There are no FlexCAN signals on PTB16 and PTB17 on the K64. Perhaps you need to interpolate the documentation to match your device(?)

Regards

Mark

0 Kudos
Reply