flexnvm as eeprom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexnvm as eeprom

1,682 Views
sanjayjadhav77
Contributor I

hi i am using frdm k20dm128 board i want use flexnvm as eeprom so plz reply if  any buddy have source code or any detail.

Labels (1)
0 Kudos
Reply
2 Replies

1,549 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello sanjay jadhav:

There is an application note about using Flex memory in Kinetis devices:

http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf

From your comment I assume the board is a FRDM-K20D50M. The MCU on-board is a MK20DX128VLH5. You can download the C90TFS flash driver from this link:

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe

Then once installed you will find an example for MK20DX128xxx5 in this path:

"...\Standard_Software_Driver_v1.03\C90TFS\Demos\build\MK20DX128xxx5"

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,549 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello sanjay,

Please configure Flash register refer to the reference manual -> 28.4.11.14 Program Partition Command

pastedImage_0.png


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply