flexnvm as eeprom

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

flexnvm as eeprom

1,659 次查看
sanjayjadhav77
Contributor I

hi i am using frdm k20dm128 board i want use flexnvm as eeprom so plz reply if  any buddy have source code or any detail.

标签 (1)
0 项奖励
回复
2 回复数

1,526 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello sanjay jadhav:

There is an application note about using Flex memory in Kinetis devices:

http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf

From your comment I assume the board is a FRDM-K20D50M. The MCU on-board is a MK20DX128VLH5. You can download the C90TFS flash driver from this link:

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe

Then once installed you will find an example for MK20DX128xxx5 in this path:

"...\Standard_Software_Driver_v1.03\C90TFS\Demos\build\MK20DX128xxx5"

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,526 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello sanjay,

Please configure Flash register refer to the reference manual -> 28.4.11.14 Program Partition Command

pastedImage_0.png


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复