flexcan is not working for k60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexcan is not working for k60

1,500 Views
gomathichinnasa
Contributor II


Hi,

Am working with CAN in k60 (having the two customized board ). Here am using the CAN0 (PTA12 & PTA13 pins ). And also am using the fls_flexcan_test.c. able to transmit the data , i checked with CRO , in CAN_TX pin data is coming and also CAN_RX also getting data , but the data is not receiving by controller.

*********FLEXCAN TEST PROGRAM.*********

   Message format: Standard (11 bit id)

   Message buffer 0 used for Tx and Rx.

   Interrupt Mode: Enabled

   Operation Mode: TX and RX --> Normal

   Node 2

***************************************

selected frequency (Kbps) is: 125

Data length: 1

FLEXCAN reset. result: 0x0

FLEXCAN initilization. result: 0x0

FLEXCAN mode selected. result: 0x0

FLEXCAN global mask. result: 0x0

FLEXCAN Error ISR install, result: 0x0

FLEXCAN Bus off ISR install, result: 0x0

FLEXCAN error interrupt enable. result: 0x0

FLEXCAN rx remote mai

lbox initialization. result: 0x0

FLEXCAN rx mailbox initialization. result: 0x0

FLEXCAN mailbox activation. result: 0x0

FLEXCAN RX ISR install. result: 0x0

FLEXCAN RX remote ISR install. result: 0x0FLEXCAN tx remote mailbox initialization. result: 0x0

FLEXCAN tx mailbox initialization. result: 0x0

FLEXCAN tx mailbox activation. result: 0x0

FLEXCAN TX ISR install. result: 0x0

FLEXCAN TX remote ISR install. result: 0x0

FLEXCAN started. result: 0x0

Data transmit: 0

Data transmit: 1

FLEXCAN tx update message. result: 0x0

Data transmit: 2

FLEXCAN tx update message. result: 0x0

Data transmit: 3

FLEXCAN tx update message. result: 0x0

Data transmit: 4

FLEXCAN tx update message. result: 0x0

Data transmit: 5

FLEXCAN tx update message. result: 0x0

like this am getting the output. receiving task is not working .

And also in my transceiver is not in sleep mode, i kept it as high speed mode only.

in RX-TASK

  if (_lwevent_wait_ticks(&event, 1 << RX_mailbox_num, FALSE, 0) != MQX_OK) {

     printf("\n\rEvent Wait failed");

  }

here its getting task_block.

0 Kudos
Reply
1 Reply

1,270 Views
gomathichinnasa
Contributor II

hi,

i replace this line

  if (_lwevent_wait_ticks(&event, 1 << RX_mailbox_num, FALSE, 0) != MQX_OK) {

     printf("\n\rEvent Wait failed");

  }

and put normal delay now its start to working, i mean i can receive the data

0 Kudos
Reply