flashloader_loader ran an error on the IAR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flashloader_loader ran an error on the IAR

1,631件の閲覧回数
wangb
Contributor II
  • Why do I run it on the IAR and it prompts me "Fatal Error[Pe1696]: cannot open source file "debug/flashloader_image.c .   C:\Users\wangb\Desktop\NXP_Kinetis_Bootloader_2_0_0\src\bootloader\src\bl_flashloader.c 38 "  ???  Thank you.
    123.png

0 件の賞賛
返信
1 返信

1,628件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi wangb,

   I suggest you build the tower_bootloader directly. This is the flash bootloader, and can be always used.

   flashloader_loader need to associated with flashloader, you need to build the flashloader at first, then build the flashloader_loader, these two project used together, and this is one time used, after you update the app, then your flashloader will be disappear, that's why I suggest you use the tower_bootloader.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------