flash details

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash details

2,032件の閲覧回数
vinkar
Contributor III

Hello ,

I am writing a small chunk of code on my KL05 (32KB flash).

After building, I have gioven generate .hex option. I am getting a hex file

abt 19KB. My aim is to use this to drive a sensorless BLDC. The LPC2121

uses abt 6KB of its 32KB flash. WHy is Kinetis using 19KB.

How can I look at the flash usage (does code warrior have one, a la MPLAB).

Is the hex file programmed into the controller. Or is it something else.

My code is below

#include "derivative.h" /* include peripheral declarations */

   

   

    #define uartEnable  UART0_C2 |= UART0_C2_TE_MASK| UART0_C2_RE_MASK; // UART is enabled // 

    #define uartDisable UART0_C2 &= ~ (UART0_C2_TE_MASK| UART0_C2_RE_MASK); // UART is disabled //

    #define luvOceansModeStartup

    #define normalModeStartup;

    #define startupBrakeTime 150

   

   

    void delaySet(uint8_t timerReg,uint16_t timeValue);

   

   

   

//*********************************************************//

// PWM module //

     void pwmInit(){   

            // PWM //

                //timer0 - PWM //               

                SIM_SOPT2 |= SIM_SOPT2_TPMSRC(1);   // clk source for TPM0 and TPM1 as well

                SIM_SCGC6 |= SIM_SCGC6_TPM0_MASK;   // clk gated for TPM0

                TPM0_SC = (1<<2);                   // 16 prescale factor

               

                //Pins of PWM //

                //--- alternate selection (all PWM are ALT2)---//

                PORTB_PCR6 |= PORT_PCR_MUX(1);   // U1+

                PORTB_PCR7 |= PORT_PCR_MUX(1);     // U1-

                PORTB_PCR10 |= PORT_PCR_MUX(1);  // V1+

                   PORTB_PCR11 |= PORT_PCR_MUX(1);  // V1-

                                                

                PORTA_PCR5 |= PORT_PCR_MUX(1);   // W1+

                PORTA_PCR6 |= PORT_PCR_MUX(1);   // W1-

               

                GPIOB_PDDR |= (1<<6);GPIOB_PDDR |= (1<<7);GPIOB_PDDR |= (1<<10);GPIOB_PDDR |= (1<<11);

                GPIOA_PDDR |= (1<<5);GPIOA_PDDR |= (1<<6);

               

                TPM0_C0SC |= (TPM_CnSC_MSB_MASK | TPM_CnSC_ELSB_MASK); // PWM - edge ,...etc //

                TPM0_C1SC |= (TPM_CnSC_MSB_MASK | TPM_CnSC_ELSB_MASK);

                TPM0_C2SC |= (TPM_CnSC_MSB_MASK | TPM_CnSC_ELSB_MASK);

                TPM0_C3SC |= (TPM_CnSC_MSB_MASK | TPM_CnSC_ELSB_MASK);

                TPM0_C4SC |= (TPM_CnSC_MSB_MASK | TPM_CnSC_ELSB_MASK);

                TPM0_C5SC |= (TPM_CnSC_MSB_MASK | TPM_CnSC_ELSB_MASK);

               

                                   

                TPM0_CONF |= TPM_CONF_DBGMODE_MASK; // timer runs even in debug mode //

                   

                // TPM0_SC -- turn on timer //   

            }

// PWM done //

//*********************************************************//

           

//*********************************************************//

// UART module //

           

    void uartInit(){        

         //UART configure //                   

                SIM_SOPT2 |= SIM_SOPT2_UART0SRC(1); // clk source for UART           

                SIM_SCGC4 |= SIM_SCGC4_UART0_MASK;  // clk gated for UART0               

                SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK;  // clk gated for PORTA

                SIM_SCGC5 |= SIM_SCGC5_PORTB_MASK;  // clk gated for PORTB

               

                PORTB_PCR3 = PORT_PCR_ISF_MASK|PORT_PCR_MUX(2);  // alternate - 4 //

                PORTB_PCR4 = PORT_PCR_ISF_MASK|PORT_PCR_MUX(2);     // alternate - 4 //

               

                //uartDisable;

                                       

                // 8 bits,stop bits,....etc //

                //GPIOB_PDDR

                UART0_BDH = 0x02;

                UART0_BDL = 0x22;

                UART0_C4 = 0x0F;                       

                UART0_C1 = 0x00;

                UART0_C3 = 0x00;

                UART0_MA1 = 0x00;

                UART0_MA1 = 0x00;

                UART0_S1 |= 0x1F;

                UART0_S2 |= 0xC0;

               

                //uartEnable;

            }

           

// UART done //

//*********************************************************//

           

//*********************************************************// 

// timer1 module //                        

     void ptm1Init(){    

         SIM_SCGC6 |= SIM_SCGC6_TPM1_MASK;   // clk gated for TPM0

         TPM1_SC = (1<<2);                   // 16 prescale factor        

         TPM1_CONF |= TPM_CONF_DBGMODE_MASK; // timer runs even in debug mode //        

        

         //TPM1_SC;    // start off timer //

     }

// timer1 done //             

//*********************************************************// 

//*********************************************************// 

// adc module //     

     void adcInit(){

        

     }

    

// adc done //             

//*********************************************************//      

//*********************************************************// 

// LPTMR module //     

     void lptmInit(){

     }

// LPTMR done //

//*********************************************************//                

 

//*********************************************************//

// --  timer register timerData

// bit7   bit6   bit5   bit4   bit3     bit2   bit1   bit0

//  x      x      x         x        1-ms     1-IE    1-on   1-on

//                                0-us     0-ID    0-off  0-off

// startBrake module //

     void startBrake(){

         uint8_t timerDat;    

         // ptm1Init(); // done at startup //

         // gpios set as output //

        

         PORTA_PCR5 &= ~(PORT_PCR_MUX_MASK);

         PORTA_PCR6 &= ~(PORT_PCR_MUX_MASK);

         PORTB_PCR5 &= ~(PORT_PCR_MUX_MASK);

         PORTB_PCR7 &= ~(PORT_PCR_MUX_MASK);

         PORTB_PCR10 &= ~(PORT_PCR_MUX_MASK);

         PORTB_PCR11 &= ~(PORT_PCR_MUX_MASK);

        

         PORTA_PCR5 |= PORT_PCR_MUX(0);

         PORTA_PCR5 |= PORT_PCR_MUX(0);

         PORTA_PCR6 |= PORT_PCR_MUX(0);

         PORTB_PCR5 |= PORT_PCR_MUX(0);

         PORTB_PCR7 |= PORT_PCR_MUX(0);

         PORTB_PCR10|= PORT_PCR_MUX(0);

         PORTB_PCR11|= PORT_PCR_MUX(0);

        

         GPIOA_PDDR = (GPIO_PDDR_PDD(5) & GPIO_PDDR_PDD(6));

         GPIOB_PDDR = (GPIO_PDDR_PDD(5) & GPIO_PDDR_PDD(7) & GPIO_PDDR_PDD(10) & GPIO_PDDR_PDD(11));

        

        

         timerDat = 10;

        

         //GPIOA_PSOR = (GPIO_PSOR_PTSO(5) & GPIO_PSOR_PTSO(6));

         GPIOB_PSOR = (GPIO_PSOR_PTSO(7) & GPIO_PSOR_PTSO(10));

        

         //delaySet(timerDat,startupBrakeTime);

        

         // brake - PTB7 - off,PTB5,PTB10 and PTA5 - on //

         //GPIOB_PCOR = (GPIO_PSOR_PTSO(7) & (GPIO_PSOR_PTSO(11);   // U1+ W1+

         //GPIOA_PCOR = ((GPIO_PSOR_PTSO(6));                          // V+

        

         GPIOB_PSOR = (GPIO_PSOR_PTSO(5) & GPIO_PSOR_PTSO(10));

         GPIOA_PSOR = (GPIO_PSOR_PTSO(5));

        

         // -- braking done calibration done -- //

     }

    

    

    

// startBrake done //

//*********************************************************//  

   

//*********************************************************//

    // -- start up and brake done -- //

    // -- ramp up is done next -- //

// open loop module // 

    void openLoopMotor(){

       

       

    }

   

// open loop done //

//*********************************************************// 

                                  

//*********************************************************//

   

   

//*********************************************************//

//    Usage - this function will set up the KL04 controller -        

//    Peripherals - timer0,timer1,LPTMR,ADC, and PWM.

//    Pins -

//            U1+ - Pin2 - PTB7

//            U1- - Pin1 - PTB6

//            V1+ - Pin8 - PTA6

//            V1- - Pin7 - PTA5

//            W1+ - Pin10 - PTB11

//            W1- - Pin9 - PTB10

//            ADC(U) - Pin11 - PTA7

//            ADC(V) - Pin12 - PTB0

//            ADC(W) - Pin13 - PTB1

//            ADC(Total) - Pin14 - PTB1

// UART //

//  Called from - main

//  Calls - pwmInit,uartInit,ptm1Init,adcInit,lptmInit

//*********************************************************//           

    void ucInit(){

       

        // clock initialised to 20.97MHz //

                // done //

                ptm1Init();

                uartInit();   

                //adcInit();

                //lptmInit();

                #ifdef luvOceansModeStartup

                    startBrake();

                #endif

                pwmInit();    // mask register bits before configuring //               

                //ADC configure //                   

                //LPTMR configure //                   

                //timer1 - Capture and compare from Atmega //

                //LPTMR and commutation timing  - ADC capturing //

            }

           

//*********************************************************//           

       

//*********************************************************// 

// -- delays -- //

    void delaySet(uint8_t timerReg,uint16_t timeValue){

        uint8_t mask;

        uint8_t countRegTemp;

        uint16_t timeValueTemp;

        uint16_t rough;

       

        countRegTemp = 0;

        if((mask = 1<<countRegTemp+3) == 1){

            countRegTemp = 0;

            // msecs //

            if((mask = 1<<countRegTemp) == 1){

                // timer0 on //

                TPM0_MOD = 1309;

                TPM0_SC &= ~(TPM_SC_CMOD_MASK);   

                TPM0_SC |= TPM_SC_CMOD(0);               

                for(timeValueTemp =0;timeValueTemp<=timeValue;timeValueTemp++){

                    while(TPM0_SC & TPM_SC_TOF_MASK){

                        TPM0_SC &= ~(TPM_SC_CMOD_MASK);                       

                        TPM0_SC |= TPM_SC_TOF_MASK;

                        TPM0_SC |= TPM_SC_CMOD(0);

                    }

                }

            }

            else{

                // timer 1 //

                TPM1_SC &= ~(TPM_SC_CMOD_MASK);   

                TPM1_SC |= TPM_SC_CMOD(0);   

                for(timeValueTemp =0;timeValueTemp<=timeValue;timeValueTemp++){

                    while(TPM0_SC & TPM_SC_TOF_MASK){

                        TPM1_SC &= ~(TPM_SC_CMOD_MASK);                       

                        TPM1_SC |= TPM_SC_TOF_MASK;

                        TPM1_SC |= TPM_SC_CMOD(0);

                    }

                }

            }

        }

        else{

            // usecs - look if its a multiple of 10 //

            if(timeValue <10){

                timeValue = 10;

            }

            rough = timeValue%10;

            if(rough != 0)

                timeValue = ((timeValue/10)*10);

            if((mask = 1<<countRegTemp) == 1){

                // timer0 on //

                TPM0_MOD = 13;

                TPM0_SC &= ~(TPM_SC_CMOD_MASK);   

                TPM0_SC |= TPM_SC_CMOD(0);               

                for(timeValueTemp =0;timeValueTemp<=timeValue;timeValueTemp++){

                    while(TPM0_SC & TPM_SC_TOF_MASK){

                        TPM0_SC &= ~(TPM_SC_CMOD_MASK);                       

                        TPM0_SC |= TPM_SC_TOF_MASK;

                        TPM0_SC |= TPM_SC_CMOD(0);

                    }

                }

            }

            else{

                // timer 1 //

                TPM1_SC &= ~(TPM_SC_CMOD_MASK);   

                TPM1_SC |= TPM_SC_CMOD(0);   

                for(timeValueTemp =0;timeValueTemp<=timeValue;timeValueTemp++){

                    while(TPM0_SC & TPM_SC_TOF_MASK){

                        TPM1_SC &= ~(TPM_SC_CMOD_MASK);                       

                        TPM1_SC |= TPM_SC_TOF_MASK;

                        TPM1_SC |= TPM_SC_CMOD(0);

                    }

                }

            }

        }       

    }

   

// -- timer delay done //

//*********************************************************// 

   

   

   

   

    int main(void)

    {

        // initialise //

        ucInit();

        //pwmInit();

        openLoopMotor();

        while(1){

            //closedLoopMotor();

        }

       

        //return 0;

    }

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,822件の閲覧回数
xiaodong_zhang
NXP Employee
NXP Employee

hi karuvat,

    Please make sure optimization level chosen by you is optimize size(-Os).

pastedImage_0.png

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,822件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Please check your project compile generated map file about memory usage.

I suggest to use CodeWarrior GCC compiler, which has higher compile performance for Kinetis product.

Wish it helps.

Best regards,

Ma Hui

0 件の賞賛
返信