firmware upgradation over Air

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

firmware upgradation over Air

1,502 Views
mayursavaj
Contributor III

Hi All,

I am working as firmware Developer. We are working on Cortex M4 Series micro controller (MK22Fx512).

Is there any method to upgrade firmware over the Air? Our device have GPRS Connectivity.

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Reply

1,272 Views
Rick_Li
NXP Employee
NXP Employee

Hi Mayur Savaj,

the below is the link for AN2295 which is on developing a serial bootloader.

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf

you can also download the corresponding SW for AN2295 by searching AN2295SW in Freescale website.

Here suppose your GPRS module is connected to MK22 by using a serial port.

if you can reset the MCU, then, by transfer data via GPRS, you may update the firmware.

I hope it helps!

0 Kudos
Reply