error when connecting K40 kinetis kwikstik by external segger jlink using KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error when connecting K40 kinetis kwikstik by external segger jlink using KDS

2,749 Views
lijofrancis
Contributor III

Dear Sir

I am using kinetis keikstik board.i can debug this board using internal segger jlink.Then i tried to connect external segger jlink jtag .

i make switch position (off) to use extenal jtag. applied 3v enernal jtag power.there i got error

launching the project encountered problem

error in final launching sequence

"

Failed to execute MI command:

-target-select remote localhost:2331 "

on console there is

"Quit (expect signal SIGINT when the program is resumed)"

please tell me solution

0 Kudos
Reply
3 Replies

2,532 Views
ivadorazinova
NXP Employee
NXP Employee

Dear Lijo Francis,

please, what is your reason for the external segger jlink when the segger jlink is on a board?

Best Regards,

Iva

0 Kudos
Reply

2,532 Views
lijofrancis
Contributor III

Dear sir,

The problem solved .The external jtag port to program external controller. We try to program board controller using external programmer. So I make the switch to On position and give VSS (gnd)directly programmer connector. So thank you for your response

0 Kudos
Reply

2,529 Views
lijofrancis
Contributor III

Dear sir,

I am working in Research and development company ,CDAC,India.We actually buy this eval-board(kinetis kwikstik) to use our project using the microcontroller that used in the Tower board. So we have to test external segger jlink programmer that already we have.So please tell me as soon as possible.

0 Kudos
Reply