eGUI release

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eGUI release

9,087 次查看
Thommi_Tulpe
Contributor IV

Hello,

when can I download a new release of the 

eGUI.

 

I have the version v2_24.

 

Best Regards

Thomas

,

 

0 项奖励
回复
15 回复数

8,019 次查看
Gargy
NXP Employee
NXP Employee

Hi,

you have +- latest version 2.24.

Be patient, I hope that we will prepare in Q1 some major update of eGUI and we will released it on the web.

At the moment we were gathering the new work requestes and also bugs reports :smileyhappy:.

 

Gargy

0 项奖励
回复

8,019 次查看
Thommi_Tulpe
Contributor IV

Hello Gargy,

thank you for the request.

The most things i need worked well.

I only have a problem with the cursor in the console.

So if the d4d_console.c and .h is ready i would like to test the files.

The problem was because the line count.

(static D4D_CNSL_DATA name##_data = { /*line_cnt - 1*/ 0, {0, 0}, D4D_FALSE, 0, 0}:smileywink:

 

Best Regards

 

;

0 项奖励
回复

8,019 次查看
Gargy
NXP Employee
NXP Employee

Hi,

 The problem with cursor is fixed. It will be available in next release. Hope soon.

Gargy

0 项奖励
回复

8,019 次查看
Thommi_Tulpe
Contributor IV

Thank You,

will you please post here, if the release is available ?

 

Best Regards

Thomas

0 项奖励
回复

8,019 次查看
Gargy
NXP Employee
NXP Employee

Hi, it will be really soon.

More functionality, less examples. Just one example for Kinetisk60/K70 and one for ColdFire.

Gargy

0 项奖励
回复

8,019 次查看
Thommi_Tulpe
Contributor IV

Hi Gargy,

when can I use the new release of the eGUI.

You told the bug in the console is fixed.

If the release is not ready, can I change the files d4d_console.c and d4d_console.h  in the old version of the eGUI

with your help ?

 

Best Regards

Thomas

0 项奖励
回复

8,019 次查看
Nouchi
Senior Contributor II

Hi,

 

Any news about new EGUI release?

0 项奖励
回复

8,019 次查看
Gargy
NXP Employee
NXP Employee

Hi,

 I know that I promise some time ago that the eGUI will be really soon and there is still nothing. :smileysad:

 

But at the moment I have finished eGUI itself and I just work on new example and update of documentation, so the time of release is pretty close.

Colleague have  to also finish new version of converter utility and we will do final test of external fonts support.

Please be patient and I hope that you will be satisfied with all new features.

0 项奖励
回复

8,019 次查看
Maciek
Contributor V

Hi,

 

what about the new release of eGUI software ?

What new features will be available and when ?

('when' is most important...)

 

Best regards

Maciek

 

0 项奖励
回复

8,019 次查看
Gargy
NXP Employee
NXP Employee

HI,

 at the moment we are finishig the release package of new eGUI 3.00, if you are interested to get the any early release package send me the private message with your email, description of your application with eGUI, and your company.

 

Best regards

Gargy

0 项奖励
回复

8,019 次查看
hl
Contributor II

Hi Petr,

I want to use the build-in LCD controller of the K70 and are looking for the new eGUI 3.0.

Can you give the date of release in the meantime, or is it possible to get a pre-release?

[email protected]

Best regards

HL

0 项奖励
回复

8,019 次查看
usm-els-tn
Contributor I

eGUI Release discussion on the Freescale Community

Hi,

Actual I'm working with the TWR-K60N510 and I'm looking for a smart solution to support a customer LC-Module (200x80 dots with an UC1618T controller).The communication with the LC-Module shall be done by SPI @ K60

Therefore I would like to evaluate your eGUI 3.0 for an upcomming project using Kinetis K60.

Would you be so kind to send me a pre-release to the following email address?

[email protected]

Thanks in advance.

Best Regards

Thomas

0 项奖励
回复

8,019 次查看
firebrizz
Contributor II

any news about release date of eGUI 3.0?

0 项奖励
回复

8,019 次查看
Nouchi
Senior Contributor II

Hello Gargy,

 

It would be nice for future release, to find file selector, and virtual keyboards, and a new focus scheme.

I explain :

- no object focussed by default.

- object focussed  when pressed, and redrawn  before *_OnClick*() call.

- object unfocussed and redrawn when it's released or after adjustable time.

It would be nice to have touch screen behaviour like android or other tactile devices.

0 项奖励
回复

8,019 次查看
J2MEJediMaster
Specialist I

You might want to take a look at this web page. It has version 2.07.

 

---Tom

0 项奖励
回复