eFlex PWM Using DMA Not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eFlex PWM Using DMA Not working

2,843 Views
OnoFame
Contributor II

Hello everyone, I am having issues getting eFlex PWM to work on the MKV44F128VLH16

The packet length is 384 and it is 16-bit. I need to send this to the register continuously.

Can anyone help me please?

0 Kudos
Reply
2 Replies

2,799 Views
_Leo_
NXP TechSupport
NXP TechSupport

Thank you so much for your interest in our products and for using our community.

I am sorry to inform you that so far we do not have that specific example code with the PWMA/eFlexPWM module.

The closest I've found to what you're looking for, which you could use as a reference, are the application notes AN5121 and AN4598, as well as the SDK example evkbimxrt1050_qtmr_inputcapture_outputpwm_dma. Although I must clarify that they are for other devices.

Please excuse any inconvenience this may cause you.

Have a nice day!

0 Kudos
Reply

2,777 Views
OnoFame
Contributor II
Hi NXF86756, I will be looking at this application notes and I will get back to you. Thanks a lot for your help so far.