does the Kinetis K81 USB suspend is available when connected with Android device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does the Kinetis K81 USB suspend is available when connected with Android device?

1,792 Views
robinliao
Contributor I

Hello NXP

Is the usb pause mode available when connected to an Android phone/tablet?

I have implemented the USB suspend function on our device and it works fine

my usb devices can be suspended/resume when connected to the host PC

but when I connect to the Android phone, the usb device is always running, and will not enter the USB suspend state

How to configure the usb library to support usb suspend on Android devices? Or is this problem based on the Android configuration?

 

Thanks

Robin

0 Kudos
Reply
2 Replies

1,747 Views
robinliao
Contributor I

it looks like USB autosuspend did not enabled on the Android device?

thank you for your response

0 Kudos
Reply

1,759 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Robin,

We do not have specific configuration for Android devices in our USB stack, therefore, I think the problem could be on the Android side, maybe there is a some driver missing.

Best regards,

Felipe