does the Kinetis K81 USB suspend is available when connected with Android device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

does the Kinetis K81 USB suspend is available when connected with Android device?

1,791件の閲覧回数
robinliao
Contributor I

Hello NXP

Is the usb pause mode available when connected to an Android phone/tablet?

I have implemented the USB suspend function on our device and it works fine

my usb devices can be suspended/resume when connected to the host PC

but when I connect to the Android phone, the usb device is always running, and will not enter the USB suspend state

How to configure the usb library to support usb suspend on Android devices? Or is this problem based on the Android configuration?

 

Thanks

Robin

0 件の賞賛
返信
2 返答(返信)

1,746件の閲覧回数
robinliao
Contributor I

it looks like USB autosuspend did not enabled on the Android device?

thank you for your response

0 件の賞賛
返信

1,758件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Robin,

We do not have specific configuration for Android devices in our USB stack, therefore, I think the problem could be on the Android side, maybe there is a some driver missing.

Best regards,

Felipe