differences bewteen k53 k60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

differences bewteen k53 k60

1,861 次查看
ednasalazar
Contributor II

Hi everbody,

I developped SPI, UART I2C, interfaces using TWR-K60N512, however if i try to change of µC (K53) using TWR K53 it doesnt work.

Can somebody explain me what is it the difference between both µC?

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,675 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi edna salazar,


please, can you specify what does not work?

TWR-K60N512 and TWR-K53N512 are similar devices.


Both of them have 3x SPI modules, 2x I2C modules, 6x UART modules, SDHC and I2S module communication interface.

TWR-K60N512 has Two Controller Area Network (CAN) modules in difference with TWR-K53N512.


So, it should works.


I attach you the comparison.

hw.png

You can try our Product Selector Freescale Product Selector


Best Regards,

Iva




1,675 次查看
ednasalazar
Contributor II

Hello Iva,

Thank you very much for your help.

However I found that the main difference between  both µC is the clock configuration and the clock associated with each module.

0 项奖励
回复