default analog pin needs pull-up or pull-down?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

default analog pin needs pull-up or pull-down?

2,192 Views
okubohitoshi
Contributor I

When the pin muxing mode is configured for analog pin (default), the port needs pull-up or pull-down resistor ?

Labels (1)
0 Kudos
Reply
3 Replies

1,989 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello okubo:

If configured for analog, the internal pullup/pulldown settings have no effect and they are disabled.

Or maybe you refer to a need for external resistors?

Regards!

Jorge Gonzalez

0 Kudos
Reply

1,989 Views
okubohitoshi
Contributor I

Thank you.

However, it is that I want to ask is that it need a external resistor for safety.

Is there trouble in unconnected unused pins of the default settings?

0 Kudos
Reply

1,989 Views
Jorge_Gonzalez
NXP Employee
NXP Employee


Hi okubo:

You do not need pullup/pulldown resistor in unused pins. It is recommended to leave them floating and configured as disabled (default).

Hope this clarifies your doubt.

/Jorge Gonzalez

0 Kudos
Reply