daughtercard for Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

daughtercard for Kinetis

3,297 次查看
drazenletina
Contributor II

Hello ,

by reading the TWRKV31F120MIARUG.pdf  I have notest that pcb TWR-KV31F120M has mounted daughtercard on it ( see page 4/10 of TWRKV31F120MIARUG.pdf  ).

I would appreciate any information about this daughtercard ,i.e. link to  schematic ,  Freescale code  of this daughtercardand also if it is possible to order few pcs from Freescale or from some distributor ( in Europe ).

Thank you ,

Drazen Letina

0 项奖励
回复
6 回复数

3,163 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Drazen and Mark,

If you turn aside the the board, you can see the J500 40 pins female connector(motor control connector from the top side perspective), you can connect power stage board with the J500 connector.

Hope it is helpful inf.

BR

XiangJun Rong

0 项奖励
回复

3,163 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Drazen and Mark

For the motor control power stage board, there are two connection methods:

1)the latest connection is to use the following boards: TWR-KV31F120M(control board), TWR-MC-LV3PH(power stage board), TWR-ELEV(primary and secondary boards), as far as I know that the TWR-MC-LV3PH kit includes BLDC motor with Hall sensor, 24V DC power supply. with this connection, you can establish a typical motor control system.

2)the old connection is to use the following boards:TWR-KV31F120M(control board) plus APMOTOR56F8000 motor control Demonstration board. You can order the APMOTOR56F8000 motor control Demonstration board from the website:

http://tinyurl.com/pdprvhc

anyway, I suggest you use method 1, order TWR-KV31F120M(control board), TWR-MC-LV3PH(power stage board), TWR-ELEV(primary and secondary boards) to establish BLDC motor control system, with this system, you can use many other control board to control the BLDC motor, for example TWR-8400(MC56F84789)  or TWR-8200(MC56F82748) DSC control boards to control BLDC.


You can order TWR-MC-LV3PH kit from the website:

http://tinyurl.com/kz2rm5o


you can order the TWR-ELEV(this is a flank boards including primary and secondary boards) from the website:


http://tinyurl.com/myc69y3



BR

XiangJun Rong

0 项奖励
回复

3,163 次查看
mjbcswitzerland
Specialist V

Hi Drazen

I thik that you need to post the version of the document that you have or a link to it because there is no doughter board on the picture on that page in the version at Freescale: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRKV31F120MIARUG.pdf

Regards

Mark

Kinetis: µTasker Kinetis support

KV10: µTasker Kinetis TWR-KV10Z32 support

KV31: µTasker Kinetis TWR-KV31F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复

3,163 次查看
drazenletina
Contributor II

fromPage4_Of_TWRKV31F120MIARUG.PNG.pnghttp://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRKV31F120MIARUG.pdf

Mark , thanks on the reply.

Here is picture and the link .

For me it looks like there is daughtercard on the board , but I can not  tell that I am 100% sure.

0 项奖励
回复

3,163 次查看
mjbcswitzerland
Specialist V

Drazen

There is no daughter board on it - I have this one and it looks like that; maybe the square with rounded edges around the processor makes it look as if it higher than the rest of the board (?) but it is not.

Regards

Mark

3,163 次查看
drazenletina
Contributor II

Mark ,

thanks on the explanation.

Drazen

0 项奖励
回复