d4d.h : No such file directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

d4d.h : No such file directory

ソリューションへジャンプ
2,477件の閲覧回数
joelesco
Contributor III

Hi,

I'm using Code warrior with the TWR K70 and I would like to use eGUI. So my problem is :

- I put the D4D libraries on my project with everything !!! In the common_files there'is the d4d.h ! But when I try to use It I always have d4d.h  : No such file directory.

so I tried to enter all the path in the #include but ... nothing better !

If you have an IDEA ! I take IT !!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,289件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Add the path to the Project settings. ARM Compiler -> input

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,289件の閲覧回数
joelesco
Contributor III

Thank you for answering.

I'm sorry but I don't understand exactly where I need to add the path In the Project_Settings.

Is it in the __arm_end.c or __arm_start.c ?

Thanks again Luis .

0 件の賞賛
返信
2,290件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

The path where s4d.h is in your project.

Luis

0 件の賞賛
返信
2,290件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Add the path to the Project settings. ARM Compiler -> input

Luis

0 件の賞賛
返信