console IO interrupt uart5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

console IO interrupt uart5

ソリューションへジャンプ
1,827件の閲覧回数
Catosh
Contributor IV

Helllo,

currently I am using a TWM k60 evm module.

I would like to use the console IO component trough UART5, and I would like to be able to enable interrupts on this component.

Anyway, using ProcessorExpert, I am not able to change "Interrupt/service event" value into enable because it is disabled.

I previously enabled CPU's NMI.

I suppose is "obvious" not enabling interrupts on port used as debug purpose, but I am not sure.

Any hint would be gladly appreciated.

Best regards,

Luca.

0 件の賞賛
返信
1 解決策
1,655件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Luca,

    Yes, you are right, the console IO component  is really can't set the the interrupt function, because it is the integrated component.

    If you want to use the interruption, you can choose the "Serial_LDD" component, "AsynchroSerial" component or "Init_UART" component, these components can set the interrupts.

    You just choose wrong component.

    Wish my answer will help you!

    If you still have question, please let me know!

Best regards!

Jingjing

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,656件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Luca,

    Yes, you are right, the console IO component  is really can't set the the interrupt function, because it is the integrated component.

    If you want to use the interruption, you can choose the "Serial_LDD" component, "AsynchroSerial" component or "Init_UART" component, these components can set the interrupts.

    You just choose wrong component.

    Wish my answer will help you!

    If you still have question, please let me know!

Best regards!

Jingjing

0 件の賞賛
返信