can i program MKW41Z512 without sda controller?or direct using rs232

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can i program MKW41Z512 without sda controller?or direct using rs232

2,347 次查看
sheshnathchauha
Contributor II

hi there,

i am sheshnath chauhan and i want to know about MKW41Z512 controller programming option except sda.

Kinetis Microcontrollersdhavalkhumphrihttps://community.nxp.com/community/about

标签 (1)
0 项奖励
回复
3 回复数

2,120 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

You can use a J-LINK to program the microcontroller, as well as the OpenSDA. If you have a bootloader you could also program it with UART or SPI just as it is done with the Kinetis Wireless Host Application Programming Interface (Host API).

The Kinetis Wireless Host Application Programming Interface (Host API) implements the Framework Serial Connectivity Interface (FSCI) on a peripheral port such as UART, USB, and SPI; the documentation and the stack it’s located in the SDK of the FRDM-KW41Z that you can download from  MCUXpresso.

 

Regards, 

Estephania

0 项奖励
回复

2,120 次查看
sheshnathchauha
Contributor II

Hi

I don't have boot loader . Could you please tell me about the bootloader

and how can get it.

Thank you

On 26-May-2017 7:57 PM, "estephania_martinez" <[email protected]>

0 项奖励
回复

2,121 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

You can find more information about the bootloader in the Kinetis Thread Stack and FSCI Bootloader Quick Start Guide. 

You can find this document in the SDK release I mentioned in the first reply under the following path: 

<download path>\SDK_2.2_FRDM-KW41Z\docs\wireless\Thread\

Let me know if you have any other doubt 

Regards, 

Estephania 

0 项奖励
回复