buzz click into hexiwear program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

buzz click into hexiwear program

2,015 Views
emmanueleschali
Contributor I

Hello,

I'm sorry, i don't know if i'm in the good place to ask this, but i try.
I have two projects kds on separate workspace.
The first is hexiwear, it builds and it works and the program run on the watch
The second is buzz click it builds and it works as well and the program run on the watch, i can heard the melody with the buzz on the slot3

I should like to add the buzz function in the hexiwear program.
So i begin to merge just the main.h and i try to load the list a lib.

My problem is, when i load one of them ,
#include "fsl_enet_driver.h"
#include "fsl_ewm_driver.h"
#include "fsl_flexbus_driver.h"
#include "fsl_vref_driver.h"
#include "fsl_wdog_driver.h"

My project doesn't build and i got an error
arm-none-eabi-g++: error: CreateProcess: No such file or directory
makefile:143: recipe for target 'HEXIWEAR_MK64.elf' failed
make: *** [HEXIWEAR_MK64.elf] Error 1

Have you an idea, or maybe there is another way to do that.

Thanks for your help.

0 Kudos
Reply
3 Replies

1,915 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi emmanuel eschalier,

    When you want to merge two project together, you can't just merge the main.h.

   You also need to add the according header files to your project, and check the project headfile path in the proterties.

  You must make sure these file:

#include "fsl_enet_driver.h"
#include "fsl_ewm_driver.h"
#include "fsl_flexbus_driver.h"
#include "fsl_vref_driver.h"
#include "fsl_wdog_driver.h"

The according header file source code add to your project.

Please check it at first, I don't have the hexiwear board, but I think your problem is just the two project merge problem.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,915 Views
emmanueleschali
Contributor I

Hello Kerry Zhou,

Thank you for your quick answer .

I know that is not enough the merge the main.h to merge to project but i wanted begin by that :smileyhappy:

So Which header files do you mean ?

0 Kudos
Reply

1,915 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi emmanuel,

     I just mean the header files you add, when you add it in your project, you must make sure that header file is really copied to your new project. And the path also need to add it in the IDE project.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply