bootload for k60 use by serial port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bootload for k60 use by serial port

10,197件の閲覧回数
李志權
Contributor II

I have searched an2295

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf?&Parent_nodeId=&Parent_pag...

https://community.freescale.com/docs/DOC-95039

But I only find the IAR and KEIL projects inside, had not found the cw,

Can provide a project of the cw?

Or tell me how to create the bootload projects?

I use the development board is TWR - K60D100M

The cw version is 10.4

ラベル(1)
0 件の賞賛
返信
21 返答(返信)

275件の閲覧回数
李志權
Contributor II

Thank you, now compile successfully.

Then, I opened the win_hc08sprg this program and want to download an application, see if I can run correctly

But I have two questions here:

1. How to generate the S19 file

2. How to set up the application of engineering, it can be downloaded in down after, can run successfully, such as how to set the interrupt table, how to set up the LCF file?

0 件の賞賛
返信