blhost linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

blhost linux

2,813 Views
LArmstrong1985
Contributor III

Hi,

I was able to port the bootloader and buspal to my custom board.

With blhost on Windows all works perfect and I can program my board via CANBUS.

On Linux, I tried several version (KBOOT 2.0, MCUBOOT 2.7 and this version modified by an user (blhost-modified)) but none work properly. The main problem seems to be in receiving the replies on UART from the blhost.

My final goal is to program my board from Raspberry. I read on MCUBOOT 2.7 manual that blhost support also ARM-based Linux but in the packet MCUBOOT_2.7_FRDM_KW36 I don't find this binary (is present only i386 or amd64 version). Where I can find it? In this version, among other things, I do not find the sources of the blhost as opposed to version 2.0. Can you provide me both?

Thank you very much!

 

0 Kudos
Reply
1 Reply

2,793 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello LArmstrong1985

Hope you are well. I believe this has been answered in this post: https://community.nxp.com/t5/i-MX-RT/blhost-and-sdphost-for-ARM-Linux/m-p/935740

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply