audio sample code available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

audio sample code available?

Jump to solution
3,364 Views
bowerymarc
Contributor V

I was reading the audio slide show presentation "Introduction to MCU Audio and USB Audio Streaming"  (http://2012ftf.ccidnet.com/pdf/0110.pdf) and I'm wondering if the code for the SoundBar Surround Processor (p.60), Headphone Audio Processor (p.61) and/or Kinetis K40 Tower SRS WOW HD SoundBar Decoder are available somewhere?

thanks,

Marc

Labels (1)
0 Kudos
Reply
1 Solution
2,794 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Marc,

Sorry for the delay. The SoudBar project was the the first Audio example created for Kinetis.

Unfortunately, the Audio module was changed in new silicon revisions and this code won´t work for new devices.

Attached you can find a example of USB Speakers 96Khz 24-bits . Right now only works in Linux and Mac OS Lepoard .

I hope this helps,

Alejandro

View solution in original post

0 Kudos
Reply
1 Reply
2,795 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Marc,

Sorry for the delay. The SoudBar project was the the first Audio example created for Kinetis.

Unfortunately, the Audio module was changed in new silicon revisions and this code won´t work for new devices.

Attached you can find a example of USB Speakers 96Khz 24-bits . Right now only works in Linux and Mac OS Lepoard .

I hope this helps,

Alejandro

0 Kudos
Reply