alphanumeric display and sd card support on k70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

alphanumeric display and sd card support on k70

1,183 Views
sivakamasundari
Contributor I

do you have  alpha numeric keypad interface driver support on k70 platform (bare metal coding)?

if not kindly suggest how it can be done?

do u have sd card support using filesystem in k70 platform?

pl support on bare metal code  with file system for sd card interface and alpha numeric display

0 Kudos
Reply
1 Reply

1,104 Views
miduo
NXP Employee
NXP Employee

Hi,

The Secure Digital Host Controller (SDHC) module included on Kinetis supports the specification version 2.0 of SDCard.org; this specification supports SD Cards up to 32 GB. You can find this at the SDHC chapter of the K70’s Reference Manual.

As for the alpha numeric keypad, K70 do not support it directly but we had provide an GPIO expander which make this available.

http://cache.nxp.com/documents/leaflet/75016987.pdf?fsrch=1&sr=1&pageNum=1 

0 Kudos
Reply