add binary file to codewarrior project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

add binary file to codewarrior project

ソリューションへジャンプ
2,844件の閲覧回数
李志權
Contributor II

I have a binary file, want to join the codewarrior project, so, how to add, and how to use?

my cw version is 10.4

ラベル(1)
0 件の賞賛
返信
1 解決策
2,664件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

as we talked on the phone, there is no way in CodeWarrior to add a png image file in the project.

since CodeWarrior can't resolve such a image file.

what you can do is to convert this file to a binary file and add it to project as a header file.

hope it helps!

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,664件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

hi,

please let me know your target device!

and how do you want to add the binary file. if you just want to add it to your project as a library, then, just drag and put it in the project folder.

0 件の賞賛
返信
2,664件の閲覧回数
李志權
Contributor II

My development board is TWR - K60D100 ,

now,I haved put it in the project folder

so ,how to use in my code

2.PNG.png

0 件の賞賛
返信
2,665件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

as we talked on the phone, there is no way in CodeWarrior to add a png image file in the project.

since CodeWarrior can't resolve such a image file.

what you can do is to convert this file to a binary file and add it to project as a header file.

hope it helps!

0 件の賞賛
返信
2,664件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

please tell me your phone number, I would like to call you regarding to this issue.

0 件の賞賛
返信