adc performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adc performance

1,915件の閲覧回数
joker441
Contributor I

hey guys,

 

i've a question about the adcs... in the datasheet i found that the ENOB is14.5 bits... so far so clear...

with a conversion time of 5us (according to another thread), is it safe to assume now that the adc can operate at 200khz sample rate with an effective resolution of 14.5 bits?

 

does anybody have another source for frequency/accuracy information of the kinetis adc?

 

un saludo, j

0 件の賞賛
返信
1 返信

1,466件の閲覧回数
ChrisChelmecki
Contributor I

I had a similar question, so I thought I would post my analysis even though this post is getting old.  Basically, it doesn't look like you can assume that.  In order to get the 14.5 ENOB you need to use differential mode, and set the averaging to 32 samples.  I did my calculations for single ended, which gives a max ENOB of about 13.5.

 

For a K60-100MHz part, I can set the ADC clock to a max of 6.25Mhz because the max is 12Mhz for 16bits, and there are only power of two clock dividers.  This gives me a sample+ convert time of 140.42 usec, or about 7121 ksps.  Differential is even slower.

 

If you get rid of the averaging you loose about a bit of ENOB and get a sample+convert time of about 6.5 usec, or about 154 ksps.  Differential will be a little bit slower again, and you can't switch between as many channels. 

 

You will most likely need to check the DS & RM for the specific part and check to see what you can clock the ADC at. 

0 件の賞賛
返信