actualizacion de bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

actualizacion de bootloader

2,269 Views
albertoflores
Contributor I

hola estoy usando windos 8.1  y me e fijado que hay una falla  con el bootoader de  la frdm-kl25z  busque la actualización y  ahora la  computadora la  reconoce como MBED  esto es correcto o es  otro archivo

0 Kudos
Reply
2 Replies

1,931 Views
jiunnyang
NXP Employee
NXP Employee

Hi,

I thinks you need to change your FRDM0KL25Z board to OpenSDA-debuger mode.

Please refer the below link to download OpenSDA,

http://www.pemicro.com/opensda/

And how to change to debuger mode, you can refer the Getting into Bootloader Mode in the User's Guide, then Drag/drop or copy/paste MSD-DEBUG-TRK-KEA64_Pemicro_v116.SDA the desired application to the BOOTLOADER drive.

http://www.freescale.com/files/32bit/doc/user_guide/OPENSDAUG.pdf

0 Kudos
Reply

1,931 Views
albertoflores
Contributor I

hola gracias por la info pero ese no es el problema que tengo lo que pasa es que la computadora no reconoce la tarjeta de ninguna forma y en otra pc si lo hace

gracias

Date: Wed, 11 Mar 2015 01:22:40 -0700

From: [email protected]

To: [email protected]

Subject: Re: - actualizacion de bootloader

actualizacion de bootloader

reply from Jiunn-Jye Yang in Kinetis UART Command Line Bootloader - View the full discussion

Hi,

I thinks you need to change your FRDM0KL25Z board to OpenSDA-debuger mode.

Please refer the below link to download OpenSDA,

http://www.pemicro.com/opensda/

And how to change to debuger mode, you can refer the Getting into Bootloader Mode in the User's Guide, then Drag/drop or copy/paste MSD-DEBUG-TRK-KEA64_Pemicro_v116.SDA the desired application to the BOOTLOADER drive.

http://www.freescale.com/files/32bit/doc/user_guide/OPENSDAUG.pdf

Did your question get answered?

If so, say thanks by clicking Correct Answer in the community thread!

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in Kinetis UART Command Line Bootloader by email or at Freescale Community

Following actualizacion de bootloader in these streams:

Inbox

0 Kudos
Reply