XTAL pins capacitance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XTAL pins capacitance

Jump to solution
8,341 Views
simongodfrind
Contributor II

Hello, 

We are checking our crystal parameters and we are wondering what are the XTAL pins capacitance on the MKE16FVLH16 µC.

the capacitance is not specified in the datasheet, so we looked at the IBIS model, to see that the specified value is about 0.334pF. This value seems very low. We can see that it is about the same for all other pins, but in the datasheet it is stated that digital pins usually have a 7pF capacitance, so we don't know what value to use.

What is the capacitance value for XTAL pins ?

What is the value expressed in the IBIS file ?

 

Thank you in advance,

Labels (1)
0 Kudos
Reply
1 Solution
8,190 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @simongodfrind ,

C_pkg is for those pins who haven't C_pin. Pin11 needn't C_pkg.

C_comp is different with C_pkg/C_pin. C_comp is model cap or die cap. You can add it.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
10 Replies
8,329 Views
simongodfrind
Contributor II

That's not a good answer. Please read the question.

0 Kudos
Reply
8,314 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @simongodfrind ,

I asked to designer. They said the ibis module is got by simulation. This value should be used to calculate XTAL CL. Cin_a in Capacitance attributes table should not be used.

 

Regards,

Jing

0 Kudos
Reply
8,278 Views
simongodfrind
Contributor II

Hi Jing,

Thank you for your answer but I need the advice from your team to size the right c_load for the crystal circuit in order to robustify our design before production. I understand that those values are not at hand.

According to your datasheet :

simongodfrind_0-1649059734030.pngsimongodfrind_0-1649059734030.pngsimongodfrind_1-1649059750464.pngsimongodfrind_1-1649059750464.png

So, as stated, we check the crystal manufacturer user manual and datasheet and it says this : 

simongodfrind_3-1649060420554.pngsimongodfrind_3-1649060420554.png

simongodfrind_2-1649060323255.pngsimongodfrind_2-1649060323255.png

So we lack Cin and Cout. As you can see our question is legitimate and is not answered in the datasheet nor in this forum yet.

We would like to know what are Cin and Cout (should be different).

According to the ibis file the values seems very small (0.3pF+0.3pF? ; 0.3pF+0.4pF?), in other datasheet I am used to see (4->7pF; 7->12 pF), (4 pF; 9 pF),  (9 pF; 10 pF) or (5 pF; 10 pF).

Could you please investigate ?

It is a matter of being able to start the crystal over our temperature range and at the right frequency.

Sincerely,

0 Kudos
Reply
8,263 Views
bobpaddock
Senior Contributor IV

"...order to robustify our design before...It is a matter of being able to start the crystal over our temperature range and at the right frequency."


Really the minutiae of such tiny capacitances don't make any difference compared to the board parasitics and the real world tolerances of real capacitors.  

If you really want robustness, use a MEMs and not a crystal.

If forced to use a crystal and want to make sure it ALWAYS starts, put a 10 Meg resistor across the crystal, place a current limiting resistor on the XOut pin and make sure the two external load capacitors have slightly different values.  Take what the Crystal Manufacture recommends and change the value of each by a few pf in opposite directions.  May have to swap sides if frequency is a bit off.

Failing physical failures from overdrive or being dropped, what causes the oscillator to not start is that Murphy's Law has everything perfectly balanced on both XOut and XIn.  The 10 Meg resistor and unbalanced loading caps prevent this.

8,244 Views
simongodfrind
Contributor II

In fact it depends on the order of board parasitics (depends on layout, planes and stackup) and the order of C_in, C_out. Which I would like to know they value to confidently neglect them or not. Moreover if bad tolerances occurs despites our requirement, I would consider it as a parallel problem to assess.

My concern is that almost half of the paper I see suggest to take into account C_in and C_out. Because they claim C_in and C_out might not be negligible unfortunately (cf. previous message).

I hear you well that from your point of view they are negligible (let's find out with the help of @jingpan) compared to board parasitics and tolerances.

If they are negligible that do not make any sense to use them I agree, if not it might reduce my C_load of 23%.

Thank you for your point.

0 Kudos
Reply
8,273 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @simongodfrind ,

Please use the data in ibis. In our application notes, the capacitance of the pin itself is basically ignored.

https://www.nxp.com/docs/en/application-note/AN3208.pdf

https://www.nxp.com/docs/en/application-note/AN1706.pdf

https://www.nxp.com/docs/en/application-note/AN1783.pdf

Among these docs, AN1783 is the most important I think.

Crystal oscillator circuit provides stable oscillations when gmXOSC > 5 * gm_crit. The gm_crit is defined as:
gm_crit = 4 * ESR * (2πF)2 * (C0 + CL)2
where:
1 gmXOSC is the transconductance of the internal oscillator circuit
2 ESR is the equivalent series resistance of the external crystal
3 F is the external crystal oscillation frequency
4 C0 is the shunt capacitance of the external crystal
5 CL is the external crystal total load capacitance. CL = Cs+ [C1*C2/(C1+C2)]
6 Cs is stray or parasitic capacitance on the pin due to any PCB traces
7 C1, C2 external load capacitances on EXTAL and XTAL pins

Regards,

Jing

0 Kudos
Reply
8,267 Views
simongodfrind
Contributor II

Hi @jingpan ,

Thank you for your prompt answer incl. the stability criteria.

I understand that the procedure recommended by NXP papers neglect Cin, Cout and if I want to include them, you would recommend me to use the one from the IBIS file.

So here is my last question about this IBIS file, could you please verify my understanding?

1) I would use the C_pin given at the pin 11:EXTAL and 12:XTAL (as we have the 64 LQFP)

simongodfrind_1-1649149274956.pngsimongodfrind_1-1649149274956.png

that have 3.346e-13 and 3.336e-13F respectively.

2) But do I have to take into account C_pkg, or add it?

simongodfrind_2-1649149430435.pngsimongodfrind_2-1649149430435.png

3) Do I have to take into account C_comp typical, or add it?

3.1) If I follow the model definition of p_io_5ma_model -> p_io_5p0_5ma as we use 5V

simongodfrind_4-1649149632867.pngsimongodfrind_4-1649149632867.png

3.2) If I follow the model definition of p_io_5ma_model -> p_io_3p3_5ma as I saw the clk waveform is under 3.3V

simongodfrind_3-1649149593013.pngsimongodfrind_3-1649149593013.png

Thank you for your answer, 

0 Kudos
Reply
8,191 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @simongodfrind ,

C_pkg is for those pins who haven't C_pin. Pin11 needn't C_pkg.

C_comp is different with C_pkg/C_pin. C_comp is model cap or die cap. You can add it.

 

Regards,

Jing

0 Kudos
Reply
8,156 Views
simongodfrind
Contributor II

Hi,

@jing, according to your answer, that means we have to reduce our loading capacitor of 5.3% compared to the recommended simplified dimensioning rules. Thus, if the IBIS file is accurate enough and the interpretation are correct, Cin and Cout could be, in fact, neglected in most cases (as anticipated by @bobpaddock).

Thank you for the investigation and your time.

0 Kudos
Reply
8,334 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @simongodfrind ,

You can follow the datasheet.

 

Regards,

Jing

0 Kudos
Reply