X-KW45B41Z-EVK cannot run Bluetooth examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

X-KW45B41Z-EVK cannot run Bluetooth examples

1,211 Views
MSM1
Contributor I

Hello,

I am playing with my X-KW45B41Z-EVK board. the board was running a preconfigured demo it was working fine , i was observing the advertising events.

I have flashed the beacon / adv_ext_peripheral example from SDK 2.12.7 they both not working on my board.

I have tested Led blinky , it is working fine.

Somehow when i debug both bluetooth applications the code is stuck in : fwk_platform_ics.c:

Line 318:

/* Wait for NBU / CM3 to answer but not forever */

uint32_t cnt = 0;

bool nbu_received = m_nbu_api_ind_received;

while ((!m_nbu_api_ind_received) && (cnt < MAX_WAIT_NBU_API_RESPONSE_LOOPS))

{}

 

Thanks for the help,

MSM.

 

0 Kudos
Reply
1 Reply

1,193 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me Getting Started with the KW45B41Z Evaluation Kit?

 

Specifically, section 3.3.

 

Regards,

Ricardo

0 Kudos
Reply