Write Program flash 0 IFR with flash programmer such as cyclone ACP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Write Program flash 0 IFR with flash programmer such as cyclone ACP

3,327 次查看
embeddeddavid
Contributor IV

Hi everyone,
We are currently working with MK64FN1M0VLL12 MCU and we would like to write MAC address on Program Flash 0 IFR during production with a flash programmer such as Cyclone ACP. Is there any way to do it?
Thanks a lot in advance.

标签 (1)
0 项奖励
回复
6 回复数

3,042 次查看
embeddeddavid
Contributor IV

Hi everyone,

According to PEMicro staff, it cannot be done.

Regards,

3,042 次查看
embeddeddavid
Contributor IV

Hi everyone,

I've managed to successfully write on Program Once registers using SEGGER's JLIink by configuring an Initial Sequence. Further information can be found on this thread.

Nevertheless, I'm still wondering if it is possible to do it with PEMicro's Cyclone ACP.

Regards,

0 项奖励
回复

3,042 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Thank you for sharing.

I am checking with P&E company about if Cyclone ACP tool has the same feature.

I will let you know later.

best regards,

Ma Hui

0 项奖励
回复

3,042 次查看
embeddeddavid
Contributor IV

Hi Ma Hui,

Thanks for your time. I opened a thread at PEMicro forum a week ago, but still no answer. Maybe you get luckier than me :smileywink:.

Regards,

0 项奖励
回复

3,042 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I find same topic thread from PEMicro office website, please refer that thread.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,042 次查看
embeddeddavid
Contributor IV

Hi Ma Hui,

Thanks a lot for your time. I've had a deep look at the suggested discussion in PEMicro official forum but I'm afraid the aim of the mentioned 'PA partition command' is to configure EEPROM and DFLASH sizes on those MCUs which support FlexNVM. This command is only available on those programming algorithms supporting Program flash, Data Flash and EEPROM (mainly K6xFXxxxxxx). This is not our case, since MK64FN1M0VLL12 does not support FlexNVM.

Although there is a particular command to write on EEPROM Data Set Size register on Data Flash 0 IFR (containing EEESPLIT and EEESIZE fields - DEPART and ERPART, respectively ), there seems to be no command to write on Program Flash 0 IFR registers. We are wondering if we can do this using a script somehow (or any other alternate way).

Have a nice day,

0 项奖励
回复