Will the KL03 errata (1N86K) be fixed?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will the KL03 errata (1N86K) be fixed?

1,240件の閲覧回数
andrewsterianap
Contributor I


Is there a plan to fix the errata listed in the 1N86K document for the KL03 or can we expect that these will persist indefinitely?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,142件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Andrew,

The errata will be updated if some other bugs have been verified or previous bugs have been fixed, etc.

So I'd like to suggest that the errata file is expected to have none of modification.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信