Will the KL03 errata (1N86K) be fixed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will the KL03 errata (1N86K) be fixed?

1,245 Views
andrewsterianap
Contributor I


Is there a plan to fix the errata listed in the 1N86K document for the KL03 or can we expect that these will persist indefinitely?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,147 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Andrew,

The errata will be updated if some other bugs have been verified or previous bugs have been fixed, etc.

So I'd like to suggest that the errata file is expected to have none of modification.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply