Wifi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wifi

2,810 Views
josemartinez
Contributor III

Hi everyone,

I would like to use a Wifi module but I don't have any idea about which one I should use. If someone can recommend me some wifi module, I have got the tower K60N512, is there any board with Wifi module that I can use with this tower or an evaluation board to make test in it?

Thanks

0 Kudos
Reply
3 Replies

2,657 Views
josemartinez
Contributor III

Hi,

Thanks both of you for your answer, now I'm checking different wifi modules.

Jose

0 Kudos
Reply

2,657 Views
vedad
Contributor II

Hi,

You can also check WHZ4178/WHZ4188 modules.

0 Kudos
Reply

2,657 Views
LuisCasado
NXP Employee
NXP Employee

Hi Jose,

We have several options, check TWR-WIFI boards:

http://www.freescale.com/webapp/sps/site/homepage.jsp?code=TOWER_HOME&tid=vantower

In the wireless connectivity section.

Best Regards,

Luis

0 Kudos
Reply