WiFi Enabled TWR-POS-K81

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WiFi Enabled TWR-POS-K81

1,222 Views
timroadley
Contributor I


The Kinetis MCU POS Tower System Module|NXP  looks really promising for developing an EMV certified solution.

What's the recommendation to enabling WiFi on the TWR-POS-K81?

Is there some other brand out there that makes a module I can connect to this?

Thanks in advance!

0 Kudos
Reply
1 Reply

1,155 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Tim,

 

Unfortunately we don't have any Wi-Fi we can provide.

However, we have some MCUs that include libraries in the SDK using QCA400x Wi-Fi module. Maybe you can take a look.

Qualcomm Technologies, Inc.: NXP Proven Partner


Best regards,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply