I'm using eclipse neon and GCC ARM compiler for a project with the FRDM-K64F board and using JLink. I'm having problems debugging.
The debug session starts properly and it works fine but one of the problems is that if I try to set a breakpoint after clicking "Run" then the execution does not stop at the breakpoint and after a couple of seconds eclipse shows a little "warning" icon where the breakpoint is supposed to be. I hover over the warning icon and I get the message "Breakpoint installation failed: Suspend operation timeout".
Another problem is that I can't pause the execution. If I click the "pause" button nothing happens, also nothing happens if I click "reset". The only way to stop the execution is clicking the "stop" button but that ends the debug session completely wich is very annoying.
I really don't have any idea about how to explain the issue better, this is what I'm experiencing and I'd like some guidance about knowing what is going on.
Could somebody please help? what another kind of information do I need to add to this question to help find out the problem?