Why is ClrValue() not working?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is ClrValue() not working?

1,755件の閲覧回数
cmcc
Contributor I

I am having trouble with the PPG1_ClrValue().  First I use PPG1_Disable().  That works fine.  However, when I use PPG1_ClrValue(), nothings happens.  It is the same with PPG1_SetValue().  Why are these not working?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,701件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

This PPG component works with the FTM module as the counter module or another timer and the methods SetValue and ClearValue are only valid when the module is disabled, the necessary sequence to use them is:

Disable();

ClearValue();
Enable();

Or

Disable();

SetValue();
Enable();

These methods do not write to the duty register, this means that the value of the counter for each channel remains the same after calling these methods. The methods only write to the register that changes the initial value of the channel.

I hope this information can help you.

Regards,

Adrian

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,701件の閲覧回数
cmcc
Contributor I

Adrian,

I am aware of this.  However, my PPG signal is high even when I try to clear it.  I cannot make it low.

Sincerely,

Chris

0 件の賞賛
返信