Why did "bool” cause compilation errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why did "bool” cause compilation errors

3,432 次查看
whagiew
Contributor II

hi,

I use "bool" in the s32ds.exe project, but the compiler reports an error. How do I use bool in my project?
Thanks.
Best regards
yang

5 回复数

3,252 次查看
BlackNight
NXP Employee
NXP Employee

Hi yang,

'bool' is not a keyword in the C programming language. To use it, make sure you include stdbool.h:

#include <stdbool.h>

in your sources.

I hope this helps,

Erich

3,252 次查看
whagiew
Contributor II

thanks, the problem is solved with your help.

0 项奖励
回复

3,252 次查看
bobpaddock
Senior Contributor IV

An unanswerable question is why is it 'bool' and not 'bool_t' to match <stdint.h> types? 

Inconsistencies like this are annoying.

0 项奖励
回复

3,252 次查看
danielchen
NXP TechSupport
NXP TechSupport

stdbool.h defines bool as a macro because the C standard 7.18

stdint.h defines intN_t as typedefs because the C standard 7.20

You can use one or the other to achieve the same effect, but it's better to use the proper one to your needs, you need to consider the compatibility of the your project.

Regards

Daniel.

0 项奖励
回复

3,252 次查看
bobpaddock
Senior Contributor IV

The point is 'bool' is used as a type, it should end with a _t.

The heading of 7.16 clearly states 'bool' is a type:


"7.16 Boolean type and values".

By convention macros in C are upper case then by 7.18 it should 

be BOOL, or properly BOOL_T.


We may be looking at different version of the standard as the one I'm looking at has 7.20 as:

7.20 General utilities <stdlib.h>

0 项奖励
回复