Which is Best Controller for Speaker design?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which is Best Controller for Speaker design?

1,421 次查看
sanketkulkarni
Contributor II

   I am starting a design for a 2.1 speaker or a 2.0 speaker design. I want to add Wifi and BLE capability to my speaker. I  have selected class D amplifier as TDA8954.

   But I am confused which controller should I use? 

   Please help me on the selection of Controller.

   I am designing my own PCB. So please suggest a controller and not a board.

    Also, my aim is to design a speaker with excellent bass and treble capabilities.

标记 (1)
0 项奖励
回复
1 回复

1,360 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Sanket,

NXP hasn't WIFI chip. KW and QN series device hasn't I2S/SAI interface. You have to use 2 NXP MCU and a WIFI module to build your system. If the master's job is transfer data only, you can use KL16+KW3x. If there is also sound boost/filter algorithm, you can choose K10+KW3x. If you want your system can be extended easily, you can choose RT1015/1020+KW3x.

Regards,

Jing

0 项奖励
回复