Hi Felipe !
I try to reduce overall consumption in LLS3 mode.
For some peripherals ( Like LPTIMER 0/1) I can use 32kHz clock from low frequency crystal oscillator ( ERCLK32K from RTC32Khz ).
But I'm not sure if this better than LPO ( in LLS3) and can I completely remove usage of LPO in LLS3 mode.
May be if LPO is not used for any peripheral, it switched off automatically.
Does it possible do not use LPO in LLS3 mode ? If it not used, consumption might be less.
For LLWU , LPO need if digital filter enabled. LPTIMERs can be clocked from ERCLK32K.
RTC used RTC32kHz oscillator. WDOG is not active in LLS3.
Regards,
Eugene