Which Kinetis devices have EzPorts?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which Kinetis devices have EzPorts?

1,595 Views
chadwilliams
Contributor III

I am considering a design that uses 2 Kinetis processors and having the Master MCU update the firmware on the second MCU via a spare DSPI port.

Usually this would require a custom boot-loader or implementation of JTAG, but the Ezport looks to simplify this task because its SPI.

I'm trying to select a small, low power Kinetis that has Ezport using the Parameter search tool on the Freescale website, but there is no column I can see that indicates whether or not the device is equipped with an EzPort.

Is there a list of devices that have EzPort? 

Do any of the MKL ( lower power devices ) have EzPort?

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,354 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Chad Williams:

All of the parts in the Kinetis K family have EzPort, except for K02, which is an entry level MCU.

As for Kinetis L devices, unfortunately none of them have the EzPort interface.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,354 Views
yasuhikokoumoto
Senior Contributor I

Hello Chad,

regarding MKL devices, only KL33, KL34 and KL43 seems to include EzPort.

Best regards,

Yasuhiko Koumoto.

0 Kudos
Reply