Which Kinetis devices have EzPorts?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which Kinetis devices have EzPorts?

1,597 次查看
chadwilliams
Contributor III

I am considering a design that uses 2 Kinetis processors and having the Master MCU update the firmware on the second MCU via a spare DSPI port.

Usually this would require a custom boot-loader or implementation of JTAG, but the Ezport looks to simplify this task because its SPI.

I'm trying to select a small, low power Kinetis that has Ezport using the Parameter search tool on the Freescale website, but there is no column I can see that indicates whether or not the device is equipped with an EzPort.

Is there a list of devices that have EzPort? 

Do any of the MKL ( lower power devices ) have EzPort?

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,356 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Chad Williams:

All of the parts in the Kinetis K family have EzPort, except for K02, which is an entry level MCU.

As for Kinetis L devices, unfortunately none of them have the EzPort interface.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,356 次查看
yasuhikokoumoto
Senior Contributor I

Hello Chad,

regarding MKL devices, only KL33, KL34 and KL43 seems to include EzPort.

Best regards,

Yasuhiko Koumoto.

0 项奖励
回复