Which BSP to use?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which BSP to use?

2,014 Views
michaelschwager
Contributor III

Hi, which BSP to use for the following chips?  I'm double-checking to make sure my bugs aren't related to using wrong BSP.

1. PK60N512VMD100      -- I've been using twrk60n512 since this is the chip on the TWR-K60N512 PCB.

2. MK60DN512ZCAB10R -- I've been using twrk60n512 (same as above) because it's Z

3. MK60DN512VLQ10      -- I've been using twrk60d100m

Full version of post here:

Confirming BSPs for various chips and tower system

thanks

0 Kudos
Reply
2 Replies

1,879 Views
RadekS
NXP Employee
NXP Employee

Yes, that is correct.

  1. PK60N512VMD100 -- twrk60n512 missing "D"
  2. MK60DN512ZCAB10R -- twrk60n512 (same as above) because it's Z
  3. MK60DN512VLQ10 -- twrk60d100m Rev 2.x of Kinetis K60

I would like to recommend our application note AN4445 Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide for more details:

http://www.freescale.com/files/32bit/doc/app_note/AN4445.pdf

Simplest exact identification is trough maskset:

xM33Z and xN30D refers to twrk60n512

xN22D refers to twrk60d100m


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,879 Views
michaelschwager
Contributor III

Thank you! :smileyhappy:

Sent from my Windows Phone

0 Kudos
Reply