Where is the comparator input?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the comparator input?

ソリューションへジャンプ
2,116件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I read on the Figure 36-1 of the RM for the K60 the two comparator's input selectable through VRSEL are Vin1 and Vin2.

In my understanding should be somewhere in the pinout of the uC. I don't find.

Maybe there is a good reason why are not there....

Thank You

タグ(3)
1 解決策
1,975件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro,

There is more info regarding Vin1 and Vin2 in Chapter 3, please kindly refer to the following for details.

1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,976件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro,

There is more info regarding Vin1 and Vin2 in Chapter 3, please kindly refer to the following for details.

1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,975件の閲覧回数
pietrodicastri
Senior Contributor II

Yes

Thank You

0 件の賞賛
返信