Where is it described how KL17 inhibits interrupts while in an interrupt?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is it described how KL17 inhibits interrupts while in an interrupt?

1,162件の閲覧回数
rickstuart
Contributor V

I ask because we are debating how interrupts work on a KL17.  Obviously an interrupt which vectors to the appropriate interrupt routine is somehow inhibited by processor hardware to repeat the process.   Otherwise an interrupt would endlessly vector to the interrupt handler until the stack blows up.   I believe this processor hardware inhibiting is active until the interrupt routine is returned from.  I would be very grateful if someone could point out where this is actually described in the KL17 documentation.

タグ(1)
0 件の賞賛
返信
1 返信

1,003件の閲覧回数
dereksnell
NXP Employee
NXP Employee

Hi Rick

The KL17 is built on the Cortex-M0+ core. And all the Cortex-M cores use the Nested Vector Interrupt Controller (NVIC) to manage Interrupt sources and priorities. The NVIC is documented in ARM's core documentation found below

And I also see Earl has already provided you a detailed description at your other post

Will the KL17 allow higher priority interrupts to interrupt a lower priority interrupt?

M0+ User Guide

http://infocenter.arm.com/help/topic/com.arm.doc.dui0662b/DUI0662B_cortex_m0p_r0p1_dgug.pdf

Thanks

0 件の賞賛
返信