Where can I get Freescale's "OpenSDA Developer's Guide"?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where can I get Freescale's "OpenSDA Developer's Guide"?

跳至解决方案
1,969 次查看
NNeff
Contributor III

I saw a mention of the "OpenSDA Developer's Guide", and it sounds like just what I need.  It comes up as a search term when one types OpenSDA in the search box on Freescale.com, but I can't find it in the search results, only the User's Guide which is minimal.  Searching on just "OpenSDA" brings up 247 results.  Can anyone tell me where I can get the Developer's Guide, or attach it to a reply to this post?  Thanks!

标记 (1)
1 解答
1,410 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Nancy:

Apart from Yasuhiko and Iva's helpful answers, the next document should clarify a little bit this:

OpenSDAv2

The document you refer was not released due to the first version of OpenSDA being P&E proprietary.

Now OpenSDAv2 is open source and it is developed by the mbed community.

Regards!

Jorge Gonzalez

在原帖中查看解决方案

0 项奖励
回复
8 回复数
1,410 次查看
NNeff
Contributor III

I found the reference to the Developer's Guide, in TKW2x_OSDAUG.pdf: 

"This document provides information required to operate OpenSDA. Information on how to integrate OpenSDA into a custom hardware design and how to create custom OpenSDA applications can be found in the OpenSDA Developer’s Guide (available October 2012)."


Did such a document ever become available?  If not, where is the best place to find info on "how to create custom OpenSDA applications"?

0 项奖励
回复
1,410 次查看
yasuhikokoumoto
Senior Contributor I

Hello Nancy,

it would be this http://cache.freescale.com/files/32bit/doc/user_guide/OPENSDAUG.pdf .

Best regards.

Yasuhiko Koumoto.

1,410 次查看
NNeff
Contributor III

Thanks Yasuhiko, but what you are referencing is the User's Guide, which is short and doesn't say anything useful about developing custom apps for OpenSDA.  I'm looking for a document called "The OpenSDA Developer's Guide."

0 项奖励
回复
1,411 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Nancy:

Apart from Yasuhiko and Iva's helpful answers, the next document should clarify a little bit this:

OpenSDAv2

The document you refer was not released due to the first version of OpenSDA being P&E proprietary.

Now OpenSDAv2 is open source and it is developed by the mbed community.

Regards!

Jorge Gonzalez

0 项奖励
回复
1,410 次查看
NNeff
Contributor III

Hi Jorge,

That community discussion IS very helpful--thank you.  The mbed community is certainly productive and an asset to the ARM community.

Thanks for your answer,

Regards,

Nancy

0 项奖励
回复
1,410 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Nancy Neff,

maybe you find useful this thread. OpenSDA Developer Guide

I hope it helps,

Iva

1,410 次查看
NNeff
Contributor III

Thanks Iva.  That's frustrating info though!

0 项奖励
回复
1,410 次查看
yasuhikokoumoto
Senior Contributor I

Hello.

I think it would be the document which several times had been referred in the community.

As you say, there is no useful information in it,

However, it is hit when searching "OpenSDA Developer's Guide" in several search engines.

I'm sorry but I can no more help you.

Best regards,

Yasuhiko Koumoto.

0 项奖励
回复