Where can I buy SWD cable for FRDM-KL25Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I buy SWD cable for FRDM-KL25Z

Jump to solution
6,160 Views
kai_liu
Senior Contributor I

Well, the SWD socket on FRDM-KL25Z seems small. I can not find its cable, socket.

Does anyone know its sources?

Thanks in advance.

Tags (1)
1 Solution
5,059 Views
BlackNight
NXP Employee
NXP Employee

Farnell/element14 part numbers and links are provided here:

Completing the FRDM-KL25Z Board | MCU on Eclipse

View solution in original post

0 Kudos
Reply
10 Replies
5,059 Views
kai_liu
Senior Contributor I

Finally I decided to order them (2x5 dual line through hole 1.27mm pin header and 1.27 10pin one-to-one cable) via taobao.com to a local trader.

Pricing: 0.3 USD for pin header and 1USD for cable, for 1pcs.

Thanks for all your information.

0 Kudos
Reply
5,059 Views
pgo
Senior Contributor V

Hi Pavel,

See this page for some suggestions for Element-14 parts.

USBDM: Setting Up the FRDM-KL25Z

Prices a bit cheaper than above :smileyhappy: but the cable is shorter I believe.

bye

0 Kudos
Reply
5,059 Views
kai_liu
Senior Contributor I

sourceforge is blocked in China. :smileyangry:

0 Kudos
Reply
5,059 Views
pgo
Senior Contributor V

Some Element-14 Part Numbers

Element-14 #681-1184.

Element14 #2144328.

bye

0 Kudos
Reply
5,060 Views
BlackNight
NXP Employee
NXP Employee

Farnell/element14 part numbers and links are provided here:

Completing the FRDM-KL25Z Board | MCU on Eclipse

0 Kudos
Reply
5,059 Views
pavel_sadek
NXP Employee
NXP Employee

Hi

in the reference manual you can find this statement:

 

Note that J6 is not-populated by default. A Samtec FTSH-105-02-F-D or compatible connector can be added to the J6 through-hole connector. A mating cable, such as a Samtec FFSD IDC cable, can then be used to connect from the OpenSDA of the FRDM-KL25Z to an off-board SWD connector.

so I would recomend to contact SAMTEC!

Pavel

5,059 Views
kai_liu
Senior Contributor I

First of all Samtec product FTSH-105-02-F-D is not available from element14 any more. And I found other similiar products are very exepensive for a connector. It seems I have to find it in China anyway.

0 Kudos
Reply
5,059 Views
Mario_Guardado
Senior Contributor I

Hi

In case you need few pieces, you can order free samples directly in the Samtec webpage. For connectors and cables.

I have ordered some FFSD-05-D-06.00-01-N/FFSD-10-D-06.00-01-N cables, and FTSH-105-02-F-D   pin headers.

I hope it helps.

5,059 Views
kai_liu
Senior Contributor I

Free sample! Really great.

0 Kudos
Reply
5,059 Views
kai_liu
Senior Contributor I

Thanks. I found it already.

0 Kudos
Reply