When the NFC_CSx signals are activated ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When the NFC_CSx signals are activated ?

1,080 Views
tiborsomogyi
Contributor III

Hi, I would like to interface an array of NAND Flash Memories to an MK60F.... which has NFC interface, provided with two NFC_CSx signals. I would need more than two of them ( at least 4 )... and I am unable to find out neither the condition under which these two NFC_CSx signals are activated, nor the way I could generate more chip select signals. Could someone help me, please ? Thanks in advance.

0 Kudos
Reply
1 Reply

1,019 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

There is no way to get current activated NFC_CEx signal from NFC register.

If customer could consider to use Flexbus module to extend external memory?


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply