What is the difference between freedom_bootloader, flashloader_loader and flashloader? Which is the truly flash-resident bootloader project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between freedom_bootloader, flashloader_loader and flashloader? Which is the truly flash-resident bootloader project

1,739件の閲覧回数
1054144848
Contributor II

I want to develop a flash-resident bootloader project, using my own board, the chip is kl17z128vfm4, because the circuit pins can not be changed, the ROM bootloader can not be used. I downloaded the kl28 SDK on the NXP official website. There are three projects under the bootloader_examples folder. I want to know which one can be used to porting the flash-resident bootloader.bootloader_examples.PNG

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,590件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi James:

Please refer to the description below:

Flashloader:  bootloader that executes from target RAM memory on either the Freedom, Tower or MAPS platform.

Flashloader_loader: bootstrap loader that executes from flash memory on either the Freedom or Tower platform. This loader copies an image of the flashloader into RAM, then executes the flashboader from RAM.

The flashboader_loader project uses the output of the flashloader build to create the flashloader image to load into RAM. For this reason, the flashloader project must be built before building the flashloader_loader project.

Regards

Daniel

0 件の賞賛
返信