What is the IO buffer propagation delay for K61 MCU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the IO buffer propagation delay for K61 MCU?

1,538 次查看
sing-yew_chan
Contributor I

Hi all,

Now I am studying the write and read timing of the DDR controller including the timing of DDR signals through the DDR PHY interface. As far as I know, the read and write timing in PHY interface can be controlled through the DDR registers. However, I cannot justify the timing of the PHY interface with the missing piece of DDR IO buffer propagation delay of the K61 MCU with part number of MK61FN1M0VMJ15.

For example, based on the datasheet for NXP IMX50 with the link to the datasheet below,

https://www.nxp.com/docs/pcn_attachments/15805_IMX50CEC.pdf 

The DDR IO buffer propagation delay is given (pg 47),

pastedImage_6.png

Hope that anyone of you guys can help to provide the IO buffer propagation delay of the K61 MCU.

Thank you very much.

Regards,

Jason 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,474 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Jason,

 

Unfortunately, we do not have the timing at that very detailed level. Instead, the datasheet contains the “output valid” specification which covers the timing specifications of the DDR controller in regards to the external signals.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复